Single- or Three-Phase, Delta or Wye: Which Power Strip Is Best For Your Equipment Load? | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

Single- or Three-Phase, Delta or Wye: Which Power Strip Is Best For Your Equipment Load?

(Tech Tips, CPI Products, Power Management) Permanent link

Power requirements at the cabinet level are becoming more demanding from a standpoint of equipment density of a single cabinet and the power input requirements of this equipment. In the past, one (or two, if redundancy is to be considered) single-phase power strips would satisfy most power needs. With the advent of sophisticated network switching, blade server technology, built in power supply redundancy, and power supply real-time load sharing/balancing to mention a few advances, placement of single-phase power strips in many instances prove inadequate to meet the increasing equipment power demands. It’s like feeding a lion a squirrel for dinner – short term burst of energy, but no stamina. Not to mention the sheer quantity of single-phase power strips needed to satisfy power requirements may prohibit their positioning within a single cabinet.

CPI Power StripSingle-phase power strips still and will always hold a strong place within a data center, but matching the power strip to the equipment density and power requirements at the cabinet level is more critical. Enter the three-phase power strip. It may provide among other configurations varied outputs on the same strip (120/208 Volt outlets), more precise load balancing of equipment-to-phase on the same three-phase circuit, and a higher output wattage capacity which will allow more equipment to be connected to the same power strip – not multiple single-phase strips.

Three-phase power strips come in two configurations – Delta and Wye. In a Delta configuration, the circuit contains 4 wires (3 hot, 1 ground). All hots are the same voltage and because there is no neutral in the wiring, all outputs will be the same as the input voltage (240 Volt in/240 Volt out). A three-phase delta power strip has the same capacity as three individual single-phase power strips. In a WYE configuration, the circuit contains 5 wires (3 hots, 1 neutral, 1 ground). Because there is a neutral, it is possible to configure buss arrangement to produce either a low voltage (120 Volt) or a high voltage (208 Volt) output within a single power strip thus allowing for much greater flexibility in applications.

CPI offers three-phase power strips in both WYE and Delta configurations. Both provide several options that fit most data center needs. Some of these include:

  • 120/208 Volt WYE and 250 Volt Delta
  • 20 Amp, 30 Amp, 60 Amp, 80 Amp, 120 Amp
  • Vertical and Horizontal (19” EIA rack-mount)
  • NEMA and IEC inlets and outlets
  • Various outlet configurations (mix of outlets)
  • Optional local and IP Metering
  • Optional magnetic breakers

See CPI's complete line of power products at www.chatsworth.com/power. If  you have questions about which power strip is best for your equipment, leave a comment below or email [email protected]. You can also call 800-834-4969. Bob Sienkiewicz, Associate Product Manager.


Posted by Bob Sienkiewicz, Associate Product Manager. at 10/11/2011 09:33:12 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email [email protected] for assistance with these matters.


2/3/2026 8:31:21 PM