CPI Enhances Design of its Snap-In Filler Panels | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

CPI Enhances Design of its Snap-In Filler Panels

(Thermal Management) Permanent link
Snap-In Filler PanelChatsworth Products (CPI) has enhanced the design of its Snap-In Filler Panels, used to fill open rack-mount spaces (U) in cabinets that store rack-mount computer servers and equipment. 

Filler Panels occupy the entire rack-mount space (U) height, eliminating leakage between stacked panels. The new design has about 44% better performance than the previous version.

Snap-In Filler Panels are used in combination with the Air Dam Kit to create an internal airflow barrier between the front and back of the cabinet. The airflow barrier blocks recirculation of hot exhaust air from the back of the cabinet to the front of the cabinet, which keeps cooling air temperatures lower because cold air goes through equipment without being pre-heated by hot exhaust air.

Use Snap-In Filler Panels in any cabinet that is equipped with 19” EIA square-punched equipment mounting rails. No tools or hardware are required for installation. More details can be found here.
 

Raissa Carey, eContent Specialist


Posted by Raissa Carey, eContent Specialist at 01/02/2014 10:36:19 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email [email protected] for assistance with these matters.


5/9/2024 9:14:42 AM