Why You Should Care About the Seismic Rating of Your Data Center Cabinet | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

Why You Should Care About the Seismic Rating of Your Data Center Cabinet

(Data Center, Environmental, Seismic Environments) Permanent link

Hospital Critical Seismic FacilitySeismic areas require specific building codes and installation requirements for public buildings to ensure the safety of people and equipment. Seismic products that will be installed in these buildings must also comply with stringent guidelines.

Set by the International Building Code (IBC) and the American Society of Civil Engineers (ASCE), these guidelines include specific calculations to prevent nonstructural components from sliding or overturning in the event of an earthquake.

According to the IBC, certain facilities such as hospitals, fire and police stations, national defense buildings and other critical facilities must remain operational during a seismic event.

To meet that need, Chatsworth Products’ (CPI) designed and tested the Z4-Series SeismicFrame® Cabinet System. The Z4-Series provides critical facility operators the confidence that their rack-mount equipment will be protected even after the most severe earthquakes.

OSHPD Pre-Approved Design Saves Time and Money

In the highly seismic state of California, the California Office of Statewide Health Planning and Development (OSHPD) reviews and approves construction designs. OSHPD OPM is the pre-approval process that allows manufacturers to submit analysis or test data prepared by a registered design professional to support design requirements of the code.

The Z4-Series SeismicFrame Cabinet recently received OSHPD OPM-0112-13, which means the design, supports and attachments of the SeismicFrame comply with the requirements of the latest California and International Building Codes for Zone 4 areas.

As a pre-approved design, the OSHPD OPM can be incorporated into construction documents, simplifying the design and approval process. In addition to OSHPD OPM, the Z4-Series SeismicFrame Cabinet was tested to meet the stringent seismic testing requirements of Telcordia Technologies GR-63-CORE, which involves putting a cabinet through a series of shaker table tests to simulate a severe earthquake.

The Z4-Series passed the GR-63-CORE test with an industry-leading 1500 lb seismic equipment load and an additional 100 lb top load for cabling.

Watch the seismic test video now.

Raissa Carey, eContent Specialist


Posted by Raissa Carey, eContent Specialist at 02/09/2015 09:29:12 AM




Comments

the TIA-942 section 6.13.5 says:
"Racks that are supported by the access floor shall be bolted to the cement slab or a metal channel secured to the slab by threaded rods that penetrate through the floor tiles"

my question: in my new Data Center in Queretaro, Mexico, city in a low seismic zone. Do I need to bolt to the concrete also all my CPI 600 mm globalframes?
Posted by: Victor Sánchez at 2/10/2015 3:26 PM


Victor, One of our tech support specialists provided this answer, "Even though you have a low seismic risk, bolting your cabinet to the concrete would be best practice. I would also recommend contacting a structural engineer to advise with correct bracing in your area."
Posted by: Kim Ream at 2/11/2015 2:08 PM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email techsupport@chatsworth.com for assistance with these matters.


8/7/2020 5:26:31 PM