| Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

Be the Superhero of Your Data Center – Here’s How

 Permanent link


Be Data Center Super Hero Blog

Data managers across the country know this story all too well: Internal CPU temperatures get too hot to operate, proper cooling isn’t achieved and finally the dreaded server failure – or even melting – actually happens.

The good news is Chatsworth Products’ (CPI) Aisle Containment Solutions can help IT professionals and data center managers to become true “superheroes.”

That’s no exaggeration.

It's been determined, between 30 and 50 percent of all data centers will run out of power and cooling within the next year, and an average of four times more cooling will be used than is actually required by the IT load. By using airflow containment, it’s possible to recapture stranded or lost capacity, all while prolonging the life of your data center infrastructure.

To put this into perspective, this could mean between $5-$25 million in savings.

AISLE_CONTAINMENT_HAC_CAB_WHT_RGB72.jpg

For example, CPI’s Cabinet Supported Hot Aisle Containment isolates hot exhaust air from IT equipment in the hot aisle and directs it back to the CRAC/CRAH through a vertical exhaust duct. 

AISLE_CONTAINMENT_FS_HAC_CAB_WHT_RGB72.jpg

Meanwhile, CPI’s Frame Supported Hot Aisle Containment is perfect for colocation facilities and data centers requiring easy roll-in/roll-out capabilities, as it combines self-closing Aisle Containment Double Door Assemblies at each end of the aisle and a Frame Supported Exhaust Duct that features an independent frame that can stand on its own, allowing cabinets with varying heights to be easily added and moved.

AISLE_CONTAINMENT_CAC_CAB_WHT_RGB72.jpg

In addition, CPI developed the Cabinet Supported Cold Aisle Containment, ideal for smaller physical footprint requirements, as it confines cold air supply to an entirely closed off area targeted at cooling IT equipment instead of the room. Custom Aisle Containment Solutions are also available, and our engineers are always ready to work with you to create the best solution for your needs.

By rescuing lost power and cooling with containment, you can defend and extend the life of your data center and become a true Data Center Superhero.

To find out how you can add more computing capacity and gain up to 12 years of extended life out of your data center cooling capacity, read CPI Global Technology Manager, Ian Seaton’s White Paper titled, “Extend the Life of Your Data Center” here.

Raissa Carey, eContent Specialist


Posted by Raissa Carey, eContent Specialist at 08/30/2013 08:48:41 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email [email protected] for assistance with these matters.


4/26/2024 12:43:42 PM