Chatsworth Products' Motive™ Vertical Cable Manager Receives Platinum Award for Breakthrough Design | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

Chatsworth Products' Motive™ Vertical Cable Manager Receives Platinum Award for Breakthrough Design

 Permanent link

CI&M Innovators Award 2017 for MotiveSince our inception, Chatsworth Products (CPI) has been a leader in cable management technologies and products. It is a large part of the CPI portfolio and we continually strive to innovate products that help alleviate our customer’s challenges. Motive Vertical Cable Manager is a key example of CPI’s continued commitment to doing just that. Its legacy built on ingenuity, CPI spent a lot of time and care into the development of Motive to make it the best cable management solution in the industry—and for our customers.

Those efforts paid off, and CPI was honored to have been presented the platinum-level award—the highest honor—for Motive at the Cabling Installation & Maintenance (CI&M) Innovators Award Ceremony on Sept. 25 during the 2017 BICSI Fall Conference & Exhibition in Las Vegas. 

Shown at right is Duke Robertson, Product Manager for Open Systems, who accepted the award.

Awarded for its breakthrough design and set of tool-less accessories, Motive is truly the first cable manager of its kind in the marketplace today. 

Key Features:

Motive features a central track system, which allows for infinite, tool-less adjustability anywhere within the cable management space. Additionally, the unique design of the accessories enable a wide range of cable management configurations that allow for direct support of cables with optimal airflow through the cable manager, preparing networks for higher wattage Power over Ethernet (PoE) applications.

More advantages include:

  • Maximum utilization of space – Central track system provides unlimited adjustability with versatile direct support for cable bundles, while allowing maximum use of interior space.
  • Intuitive, tool-less design – Accessories attach to the cable manager, enabling support and management of cables, as well as quick attachment, removal and adjustment.
  • Effortless Deployment – Superior form and functions provide quick and easy moves, adds and changes through intuitive design and tool-less adjustability.
  • Support of current and future cabling needs – Versatile configurability and fiber-friendly design mitigate poor cabling practices regarding cable slack, bend radii and cable organization.
Motive Cable Management System - 32610_32620_INSTALLED_DROPEN_RGB96.jpg

In addition, the front door of Motive features a patent-pending hinge and latch design. With its ability to open from the left or right, the door offers easy push-to-close convenience that securely locks the door into place. An integrated hook on the front door provides a dedicated space for technicians to hang a test meter.

Motive can be used with open two- and four-post CPI Racks and is available in a vast variety of heights, width and configurations, matching all facility requirements. It ships partially-assembled, requiring minimal packaging, storage space and assembly, saving users valuable time and money.

For more details about CPI’s award-winning Motive Vertical Cable Manager, visit the website.

Shannon Erdley, Public Relations Specialist 


Posted by Shannon Erdley, Public Relations Specialist  at 09/26/2017 06:26:09 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email [email protected] for assistance with these matters.


4/15/2024 11:58:31 PM