| Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X

CPI’s eConnect® PDUs and Custom Data Center Solutions Better Position Oak Ridge Schools to Become One of Nation’s Top STEM Facilities

Oak Ridge School ITWESTLAKE VILLAGE, Calif., Feb. 6, 2015 — Chatsworth Products’ (CPI) eConnect® Power Distribution Units and data center solutions played a powerful role in Oak Ridge City Schools’ 1:1 learning initiative.

Oak Ridge City Schools are some of Tennessee’s most praised learning institutions. Comprised of preschool, elementary, middle and high schools that serve about 4,700 students, Oak Ridge Schools are known for their excellence and advanced academics within the educational system.

The school district strives for the success of every student. This mission inspired the “One to One” or 1:1 initiative, in which every student will receive a Microsoft Surface tablet to use at home and at school.

To withstand the heat loads of this high-density environment, which included high-tech fiber cabling throughout, Oak Ridge Schools needed a reliable PDU with remote monitoring capabilities.

With CPIs Monitored eConnect PDUs, Oak Ridge Schools would be able to monitor and measure voltage, current, power and power factor in each cabinet. Another huge plus for Oak Ridge Schools was the daisy chaining (IP consolidation) feature of the PDUs, which allows for a connection of up to 20 PDUs using a single IP address.

eConnect PDUsCPI’s F-Series TeraFrame® Cabinets with Vertical Exhaust Ducts and custom grommets were configured to hold up to 30kW of heat load, so if power requirements for equipment go up, the eConnect PDUs will be able to withstand the high temperatures within the cabinets. eConnect PDUs were designed to withstand high heat loads of any hot aisle environment, with an ambient temperature rating of 149°F (65°C).

“It’s nice to have a single-vendor solution, so we don’t have to worry about someone else’s PDU fitting and the compatibility with the cabinet. It’s a good package to go along with the cabinet,” Robert Carneim, PhD, Supervisor of Instructional Technology at Oak Ridge Schools, said. “Setting them up inside the cabinet was also incredibly easy.”

Now with a solid and redundant data center in place, Oak Ridge Schools are technologically prepared to attempt becoming top in the nation for Science, Technology, Engineering and Math (STEM).

For more information about CPI’s eConnect PDUs and other power products, visit the website. To learn more about Oak Ridge Schools, read the full case study.

 

About Chatsworth Products 
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.

CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).

More Information
www.chatsworth.com
info@chatsworth.com
800-834-4969

Media Contact
Raissa Carey
Public Relations 
rcarey@chatsworth.com
512-591-9525

©2019 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, Motive, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. 
4/14/2021 3:45:48 AM