New Motive™ Horizontal Cable Manager Now Available | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X

New Motive™ Horizontal Cable Manager Now Available

AGOURA HILLS, Calif., Feb. 16, 2017 — Chatsworth Products (CPI) recently released its Motive™ Horizontal Cable Manager, which complements the styling of the Motive Vertical Cable Manager and provides a dedicated horizontal pathway to organize and store cables above andMotive Horizontal Cable Manager below patch panels and network switches.

Motive Horizontal Cable Manager is available in 1U, 2U, 3U and 4U heights and features a contoured, snap-on front door that swings up or down to access cables. A new solid chassis option offers a solution for applications where rack-level airflow management is required. In addition, a chassis option with cable pass-through ports is also available.

Motive provides a complete cable management solution that is highly versatile in copper or fiber optic applications. The vertical manager’s four tool-less accessories provide numerous cable segregation configurations that allow for direct support of cables with optimal airflow through the cable manager, preparing networks for higher wattage in Power over Ethernet (PoE) applications.

“Motive Cable Manager is a perfect example of CPI’s ingenuity and close relationship with customers to understand their needs to develop innovative solutions that are unparalleled in the industry,” states Duke Robertson, CPI Product Manager of Open Systems.

For more information on Motive Cable Management, click here.

 

About Chatsworth Products 
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.

CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).

More Information
www.chatsworth.com
[email protected]
800-834-4969

Media Contact
Raissa Carey
Public Relations 
[email protected]
512-591-9525

©2019 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, Motive, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. 
4/24/2024 3:15:15 PM