WESTLAKE VILLAGE, Calif., Jan. 14, 2014 – The new Build To Spec (BTS) Kit Hot Aisle Containment (HAC) Solution by Chatsworth Products (CPI) is a highly adaptable, easy-to-order, field-fabricated solution ideal for custom, retrofit applications that have a mix of cabinets in varying heights, widths and depths.
The BTS Kit is a huge advancement in data center containment. It arrives on a pallet with only eight unique components and is designed for easy installation and customization on-site.
“The BTS Kit allows you to be really flexible, whether you’re in a new or retrofit installation. The design allows you to custom-fit the containment to the cabinets in a data center environment and addresses a multitude of variables that are site-specific, while still maintaining a very effective seal to maximize performance,” Sam Rodriguez, CPI’s Product Manager of Cabinet & Thermal Solutions explains.
The BTS Kit features a ceiling- or cabinet- supported duct that is used over a contained hot aisle as part of a closed hot air return. It integrates with perimeter cooling, providing immediate improved cooling efficiency and is compatible with economization methods.
Other features include:
• Elevated, single-piece duct that allows cabinets to be removed, omitted or replaced as required
• Translucent duct and door panels that allow light to enter the contained aisle
• Doors that close automatically to maintain containment and reduce recovery time
“BTS Kit allows you to deploy the containment regardless of the dimensions of the installed cabinet and equipment,” Rodriguez states.
The durable construction and maintenance-free design of the BTS Kit provides many years of use and is made with the quality you know and trust from CPI.
CPI works closely with customers to develop personalized solutions that include a complete bill of materials (BOM) and support drawings. For more information about the BTS Kit HAC Solution, visit CPI’s
Hot Aisle Containment Solutions webpage.
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.
CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).
|
www.chatsworth.com [email protected] 800-834-4969
|
Raissa Carey Public Relations [email protected] 512-591-9525
|
©2019 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, Motive, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. |